Dear Sir,
I am from Qmax, i am using charger BQ24735 and Guage BQ40z50 for monitoring our project. I am giving 16000mv voltage,1024mA current for charging and Watchdog timer is set to 44sec. Updating current and voltage for Each 5 secs, Using the 0x0071 register in fuel guage i am getting and displaying the battery percentage. But sometimes percentage of battery its not going to change, Same Percentage is there for a long time (After 55%). If we reset the device means, it shows different percentage and Chemistry ID after 2 days it is automatically changed to some other ID. How its changing dont know clearly. (Using Chemistry ID : 100). Sometimes FET enable also not work.
So please any one specify step by step initialization process.
I followed these below procedure:
1) Set the Charging Option : b912, Charging Current = 1024mA, Charging Voltage = 16000mV, Input current = 4084mA
2) Update the Current and Voltage for each 5seconds.
3) Enabling the LED_EN (0x0027) in fuel guage.
4) Writing and Reading the 0x0071 Register from Fuel guage and getting the percentage and display.
Please specify is Device Reset / FET enable / guage enable want to include in my steps.
Thank You,
ARUNKUMAR