Hello
For our project, we have to drive 26 leds with PWM on battery in a wirstband. The leds are not always On or dimming and power consumption are really important to get a 5 days autonomy. To drive leds, we use two TLC59116 driving 13 leds each. When every leds are off, each TLC consume 15ma. We can save 5ma setting the 4th bit of mode1 to 0 but it still consume 10ma each. Is there a way to save much more current because 20ma when no leds are on is a big problem on battery (300mAh)
Thank verry much!