Other Parts Discussed in Thread: TPS3110
Dear Sir,
I am using TPS3110K33DBVR ic in my board. Reset of this IC is connected to my DSP(TMS320C6745DPTPD4) and watchdog of supervisory is connected to one of the GPIO of DSP. I am using a SPI flash for DSP code storage. My code size is 144 KB. ALso i have a 2 pin jumper between reset of supervisory to reset of DSP to isolate the reset signal wherever required.
Current problem:
After power on reset DSP has to toggle the WDI, which I have written the code to toggle at every 300ms but DSP is not able to boot because supervisory is continuously giving reset to DSP.
Please check the diagram given in data sheet. I need to know what is the time from POR to WDI toggling at the start which is indicated in circle in the figure.
Also If I disconnect reset signal(by removing the jumper) from supervisory to DSP, at that time DSP is able to boot and WDI out from DSP is coming properly. And the time between reset signal(DSP side) going high to WDI toggling is 700 ms. My doubt is whether DSP is taking more time to boot (since it is an SPI flash) and not able to toggle the WDI within the time needed for supervisory because of that supervisory is issuing the reset.
Please clarify.
Regards
Amit