This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Usage of TPS65218 in non-battery applications

Other Parts Discussed in Thread: TPS65218

Hello,

We plan to use the TPS65218 PMIC  with the AM335x processor for two different use cases:

1) +5V input supply

2) +3.3V input supply

I understand the TPS65218 is ready for industrial applications with both +5V or Li-On battery usage. 

Is there any issue using the TPS65218 with a +3.3V power supply ?

Best Regards,

Romain