Hi,
I'm planning to use the power module lmz35003 for my project . My question concerning the lmz35003 is : is it able to sink current ? for example if I connect a 12V input source to the lmz35003, and on the output of the lmz35003 I have 6 V, then if I connect a load (resistor + LED for example) between the 12 V and 6V output of the lmz35003, will it sink current ?.Thanks in advance.
Best regards