Dear all,
I'm searching for 5 different DC/DC step-Down converters for my application. These are the specifications:
Vin = 36 - 27V
Vout=
1. 12V - 3A
2. 12V - 2A
3. 5V - 3A
4 5V - 2A
5. 3.3V - 4A
Can someone help?
Best,
Cortex
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There are really a lot of possibilities there. You might try searching here to get some ideas of what we offer:
Link seems to be broken...but we have 197 possible buck converter solutions with input voltages above 30 V. Can you give us some idea about your requirements and what features you may need? Do you have a preferred control mode (voltage mode, current mode, COT?) Operating frequency, etc? That could help narrow the selection some.