Hello!
I'm having problems with font based on lm3405.
I have the boost derived from a 4.7V zener with a capacitor .01uF
capacitors are (following the data sheet naming):
C1= 10uF
C2 = C5 = 1uF
the inductor is large
When R1 = 0.8ohm
IL = 0.2V / 0.8ohm = 250mA. The average current works well. But if I put the oscilloscope SW I see I have three cycles at 100% and 0% two cycles.
but when i change and put R1 = 0.4ohm duty cycle varies permanently in SW. If I put the tip of the oscilloscope on FB I see a triangular signal 35 to 40khz that never reaches 200mV.
Does anyone have the same problem? Does anyone know what is happenning?
thanks