Dear Sir.I'm Phuoc from Vietnam.
I'm try to design and make an Flyback LED driver for my CREE CXA2520 chip .(datasheet: http://bit.ly/1IFboaf).
This project is my thesis therefore it is very important to me .i hoe that you can consult me how is good way to make it.
I have tried to use UC3842 analog chip but it is not successful.
I'm know looking for another chip from TI but there are many type of them make me confuse.
My design specification:
Input : 85-265 VAC
Output voltage: 36V
Output current: 0.5 A constant current.
Topology: Flyback
Can you recommend to me the control chip and topology?
Thanks you so much.