This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HV Phase Shifted Full Bridge in VMC mode



Hi,

I am trying to generate 12V at the output of the Kit, which runs in the VMC mode (Closed voltage loop).

The load draws arond 3 Ohm. At 355V the output voltage increases, but only up to 6V instead of 12V.

Why it does not raise to 12V?

Any advice and suggestions are welcome!

Cheers