Hello,
The TLV62080 current limit is 1.6A(min) and soft start is 100us(typ).
If we use the TLV62080 with Cout=65uF, Vout=3.3V,Vin=5V, Iout=1A.
At this condition, the inrush current will be 2.145A on the following calc.
Q=CV,
Irush = Q x dv/dt=65uF x 3.3V / 100us = 2.145A
In this case ,is the current limit of TLV62080 operated for this 2.145A inrush current?
If yes, could you please share the output voltage and current waveform example?
I would like to check we should change the device or not.
Best Regards,
Ryuji Asaka