This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LED backlight driver

Other Parts Discussed in Thread: TPS61197

I am designing an LED backlight driver.  My LED string is nominally 23.1V and 100mA.  My input voltage will vary from 19V to 27V.  I was planning on using the TPS61197 as the driver.  My question is, the device if the input voltage exceeds the 23.1 volts it will try to provide the LED string, will it cause a problem?