A.13 MaxError (0x0c)
This read-word function returns an unsigned integer value of the expected margin of error, in %, in the
state-of-charge calculation, with a range of 1% to 100%.
Max error is incremented internally by 0.05% for every increment of CylceCount after the last QMAX
update. MaxError is incremented in the display by 1% for each increment of CycleCount.
This last sentence is confusing.
Should it say some thing like "MaxError is displayed in increments of 1 %".