This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24616 charging current issue

Other Parts Discussed in Thread: BQ24616

Hi,

In our charger board, we use BQ24616. The input is 19V, We use 16.8V Li-Ion pack. 

We have 10K thermistor and connected 2.2K and 6.8K biasing resistor to it and connected to TS pin

Some charge cycles we see different behaviours. I am attaching few of them. we have set charge current to 1A. we see sudden dip in current to half or 1/3. it is not following CC, CV and termination.

Kindly advice if it is specific to the board or is it anything to do with the design.

thanks in advance

regards

subbu

 

Charge & Discharge Cycle.pdf