Team,
It has been brought to my attention that the register values from the datasheet conflict with the values provided in the BQ2419XEVM_GUI software.
See below descriptions described:
Reg01 - Bit 0 Reserved in datasheet, USB OTG Current in program
Reg01 - Bit 4-5, 10 and 11 is OTG, in software 11 is N/A
Reg05 - Bit 0 Reserved in datasheet, Fast Charge Current at Low Temp in program
Reg06 - Bit 2-4 Reserved in datasheet, IR Compensation Voltage Clamp in program
Reg06 - Bit 5-7 Reserved in datasheet, IR Compensation Resistor in program
Reg07 - Bit 4 Reserved in datasheet, Charge Voltage at High Temp in program
Reg09 - Bit 6 Reserved in datasheet, OTG in software
Which of these descriptions is correct? The datasheet or the software?
Furthermore, could you elaborate on what Reg02 Bit0 sets?
Thanks,