This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65131RGER issues under 20mA load



I am working with the TPS65131RGER converter on a custom prototype board.  Giving the converter and input of 5V, and producing +/- 15V.  Schematic is attached.  With no load, +/- 15V output is fine.  When I connect 5 op amps to the output (total of 20mA), my +15V output hangs around 4.8V and my -15V output hangs around 0V.  In the waveform is when the outputs have the issue with the light 20mA load.  I can also hear a soft high pitched hum coming from the part area when the issue is seen. 

Any help would be appreciated.  Let me know what else I can provide.