Hi,
I have my test board working fine with the UCD chip previously.
Suddenly something wrong on the board and now I'm not able to scan any UCD chip on my board.
How do I start debugging this?
I checked the V33A/V33D/V33DIO, they are 3.7V. Is this Ok?
BPCap is 1.77V.
I have the PMBus signals pulled up to 3.3V with 2kohm resistor.
The voltage level measured on the 2kohm ends are 3.3V and 0.7V.
The PMBus signals are connected to all of the UCD chip.
So what could cause the pullup drops to 0.7V?