Hey there,
I'm looking to use a TPS61070 at the moment to boost from two AAA Alkaline batteries. To be safe, I want to ensure that there is not too much noise on the output voltage with a boost from 3.2V max to 3.3V. Read through the datasheet and can't seem to see any graphs on this. Is this a feasible solution to use the TPS61070 to do this? Is there any collateral to go along to support?
My primary concern is the boost with two new AAA batteries causing a bit of noise for an amplifier in a audio application I'm working on. Any comments as soon as possible would be appreciated!
Thanks!
Evan