Hi
I have an nom. 5 Volt input source (4-8-5.3V) and would like to have 12V Output (0.2-0.5A).
I have calulated for this compoenents (Source Manual)
- 2.2uH Inductor (25mOhm DCR and 2.1A)
- 30V Schottkey Diode ( Vf 0.24V with I=1A and 0.28V with I=2A)
- Cin and Cout each 10uF Ceramic
- Rcomp = 75.25kOhm
- Ccomp= 4.7nF
On Webbench there are no ceramic cap. and the compensation feedback loop seems also not to change.....
Is there any Excel-Dokument (Maybe from a similar concept) that i can use to verify?
It seems that Webbench is not configured to calculate the feedback loop....
Thank's
Andy