This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High efficiency TI solution

Guru 29720 points

Hi Team,

My customer woud like to know high efficiency TI solution for next generation(2018) model.
The requirement is the following.
-------------------------------------
input voltage: 180~264V (AC)
output voltage: 12V (DC)
output power: 450~650W
target efficiency: 97.5% @50% load
-------------------------------------
Is there any TI solution or roadmap that meet above requirement?

Best Regards,
Yaita / Japan  disty