This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61088 missing in SwitcherPro

Other Parts Discussed in Thread: TPS61087, TPS61088

HI, we would like to use SwitherPro to design a 3.6V->6V booster. We had previously done so with TPS61087 and it gave us great results. Unfortunately TPS61088 is missing from the database. 

Is there a trick to add it or is there some update available? We would follow the ref design but are not 100% confident we know what/what to change to get Vout=6V

Alternatively, could you recommend a TPS family part that that is available in SwitcherPro that can be used to designs booster with the following parameters:

Vin 3.6-4.2V (Single cell lipo)

Vout 6V

Iout max: 4A

Thank you