This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

primary and secondary protection with BQ769x0 + BQ78350

Other Parts Discussed in Thread: BQ78350

Good morning,

I would like to design a flexible and compact primary protection circuit for a BMS. It seems the combination of the AFE ic BQ769x0 and its companion chip BQ78350 could be a suitable solution. In that case I only have to program the BQ78350 with a proper golden file during production operations, in order to set all protections and recovery features. Is that correct?

If I need also a secondary protection into the same circuit, I think it is not allowed to use the same primary protection AFE and companion chip, but I have to use a redundant solution with different components for blowing up an additional driven fuse. Correct?

Is the combination BQ769x0 + BQ78350 compliant to any standard for defining it as primary or secondary protection for a Li-ion battery pack?

Thank you very much

Matteo