I have a board using on the same I2C bus, one BQ25892 and one BQ27441. I am using BatteryManagementStudio-1.3.40 to evaluate the board. However, when I start the tool with the board connected to my computer using a EV2300 interface, the software only detect the fuel gauge IC. If I start without the board connected, I can choose charger and I see the BQ25892 but not the BQ27441.
Does anybody have a way to control both ICs simultaneously using the BatteryManagementStudio application ?