This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z60 Config unused LED output

Hi,

on my custom board I connected TS2/3/4 = PIN 11/12/13 to GND as I do not use it for LED output or sense input.

Is this hardware configuration ok or should the pins be floating when not used?

I set chg thresh 1 to 1% and chd thresh 2/3/4 to 100% but when reaching 100% I get communication problems on sm-bus.

Is it possible to completely deactivate LED 2-4 as I only use LED1?

Best regards