This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40055 EVM capacitor

Other Parts Discussed in Thread: TPS40055, TPS40055EVM-001

Hi

Our customer bought the two EVM of TPS40055 which is TPS40055EVM-001.

However the capacitor which is C16 and C17 on the EVM(#2)  is different from the following device.

#1 (One of EVM)                                       

    

#2 (another EVM)

 

I think the capacitor is right side of EVM is different from left side.

What is the part number of the capacitor (C16,C17) on the right side EVM? (Panasonic?)

Because our customer is concerned the wrong EVM or worng device.

Regards,

Koji Hamamoto