This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65217C EVM for battery power supply

Hello:

I'm evaluatuing TPS65217C EVM and all the converter/LDO outputs work as it should when either AC or USB input. But my project also requires to use battery as single supply input. I tried to supply a 3.6V2000mA voltage source to EVM from pin 3 of J2 ( BAT pin input to TPS65217C ), but no outputs at the converter or LDO pins.  The TPS65217C datasheet says,  "The system can be supplied by any combination of USB port, 5-V AC adaptor, or Li-Ion battery." Not sure what did I miss.

Please help to guide me on how to power up EVM with battery supply,  either rechargable or non-rechargable or both will be fine.

Thanks.

Eric