This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISSUE CROWBAR SENSING CIRCUIT

I am designing a CROWBAR circuit with LM4041CIM3-ADJ for one of my application. I have provided the feedback resistors with 1.223V as reference for 4.3V. But is is not working as intended. I am posting the circuit schematic. Can someone suggest the correct configuration?. The circuit is not clamping the voltage at 4.3V instead it is clamping at 3.2V. TRIAC is triggering at 3.2V.