Hello,
I am planning to use LM3481 in a non-isolated flyback configuration for an automotive application for boosting 6V crank voltage to 130V.
I have done stability analysis and need to check if my analysis is ok and the power supply will be stable.
I have attached the Mathcad file for it and also the reference app notes referred for the analysis.
Would be so helpful if someone could review it and check if it works.
Thanks,
Nishant.Flyback analysis.pptx