Hello All
I am planning to use BqStudio and from the down load page it seems that it run in XP and higher but not sure if the higher includes Win 8.1
if some one using it in Win 8.1 can confirm it runs it will be appreciated
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All
I am planning to use BqStudio and from the down load page it seems that it run in XP and higher but not sure if the higher includes Win 8.1
if some one using it in Win 8.1 can confirm it runs it will be appreciated
Regards
Hello Tom,
I'm using Windows 8.1 on a laptop. I installed bqStudio v1.3.45 successfully. However, when I run the program with a bq78350-R1 it recognizes my EV2400 and the gauge, but closes after seconds of operation. I'm using v1.3.45 because it's a known stable version on my Windows 7 desktop.
I also have the old bqEVSW (v0.9.92) installed on the laptop and I'm able to read SMBus data from the same battery (bq78350-R1) using the "bq20z95 v1.50" selected target.
Any suggestions on how to fix bqStudio?
Thanks,
Jason