Dears,
I'm using the BQ34Z100-G1 for 2 Serial Lead Acid Battery(12V/18AH).
Does BQ34Z100-G1 support this Battery capacity(24V/36AH) ? if yes, how do I set up? are there any registers can function this?
Stanley
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dears,
I'm using the BQ34Z100-G1 for 2 Serial Lead Acid Battery(12V/18AH).
Does BQ34Z100-G1 support this Battery capacity(24V/36AH) ? if yes, how do I set up? are there any registers can function this?
Stanley
my apologies, Yes, I connect them in parallel(24V/36V). so I can't connect them in parallel way when I using the BQ34Z100-G1 right ?
Stanley
Dear Thomas,
Is the any possible that you could provide me the data flash image file for 24V/36mAh battery?
Stanley
Stanley,
We do not have a default configuration for that battery setup. The device is delivered with a default configuration and there is a design example to configure the device in the datasheet. I can provide guidance, if you have problems.
Tom