Hi,
I have a buck converter using lm5085 , Vin= 72v, Vout=24v. Connection diagram is same as in data sheet. TonMin=300ns. The problem I am facing is that Inductor(12uH) is heating and melting. Can anyone help me?
Tharanathpp
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you for responding sir. I attached word schematic. Please see the attached file sir.
Vin= 24 to 72, IL= 10A Max,
Inductor part no: 2102-RC... Inductor is heating at 2.3 A itself.
Please help me
Thank you,
Tharanath
Hi, John,
I am attaching lay out of my circuit. there are two converter ,one is configurable buck and one is 12 buck , 12 v buck is working( load is less), only configurable buck has issue( left side of pdf). Please see the attached file.
Thank you,
Tharanath
I am assuming that you set your Switching frequency to ~275kHz ? Did you check to see if the power convertor is switching at your set frequency? can you cehck the switch node and confirm the converter is stable?
Thanks.
David.
I suspect the variation is due to your implementation of the external amplifier. I would implement a FB Resistor network then use an injection resistor being driven by an amplifier; into the FB node.
Having said this I do not think the voltage variation is directly causing an issue with your inductor overheating. Back to the main issue of inductor over heating. Is the inductor getting hot at Iout of 2.5A?
Hi David,
I want to know which type of current which would result inductor heating , because we kept aside the circuit for some time. Anyway yesterday we put a hat sink on mosfet and some how we could manage heat of mosfet ,but inductor still heating.
Thank you,
Tharanath
Hi David,
We measured the inductor current waveform. I am attaching the waveform. I have placed 0.025R resistor between inductor and output capacitor and measured voltage across it. Inductor current is going around 6A in the waveform. But load current is only 3A. Its just shocking to me. Very big ripple current in the inductor . I think thats why inductor heating up.Please help me. Red color waveform is voltage across .025R resistor,ie indicates inductor current. green is gate waveform. Please help me sir. I am using reduced ripple configuration ie, only one capacitor across Rfb1. I have following parameter,
Vin=48V, VOUT=24V, IL=3A, iNDUCTOR =15uH , iNDUCTOR saturation current =15A, MOSFET= FDD5614P
Thank you,
Tharanath
Thanks you,
Tharanath
Hi,
The current waveform should be triangular and not trapezoidal? The measurement may well be distorted and not real? In response to your previous question, the heating of an inductor is made of two components. DC losses relating to the RMS current and DCR of the Inductor and the AC losses which is related to the peak to peak ripple current. Just looking at the magnitude of both in your plots, I don’t see an issue (ignoring the waveform shape; if real, suggests there is an issue with your power supply). But before we confirm that, if your MOSFETs are running cooler than your inductor then we can say your inductor is heating. However, if your MOSFETs run at a higher temperature than your inductor, it maybe that the inductor is conducting hat from the MOSFET. Have you ruled this out?
Thanks.
David.
Hi David,
We check the inductor current using 0.05R also and the waveform was triangular (Without the capacitor across the RFB2) Still the FET and the inductor was heating but the converter was not stable i.e. the the frequency was not stable as you can see from the below pictures.
After experimenting we try with the capacitor across RFB2 and the converter is stable.
Regarding the heating of Inductor due to mosfet, we have provided a heat sink for the mosfet but still the mosfet and the inductor is heating up and i am not getting where the power is dissipated as the output current drawn is only 3A.
Thanks,
Tharanath
Is the MOSFET temp hotter than the inductor?
I see the Green waveform is pulsing when it should not be?
Hi David,
Thanks for your support we could understand the issue with monitoring the inductor current. When we increased the inductor value to 47uH the heating issue is solved. As the inductor current was increasing due to the on time and lesser inductor value.
Also can you suggest the variable output voltage circuitry for the with the FB pin injection method, as when we driver through the op-amp the converter is not working properly.
Hi David,
We are using 10Mhz opamp for feed back to buck controller. Is load current depend on switching frequency? When I check in DSO, Increasing load switching frequency is reducing. Theory based it is independent?
Thanks,
Tharanath
Hi,
The Frequency should increase when you apply more load. The is not a Fixed Frequency PWM Controller so variations in frequency are expected. the COT control scheme employed in the LM5085 should hold a fairly constant frequency over the load and VIN Range. When the load decreases to discontinuous current conduction (DCM) the frequency will decrease.