I ask you: often see the connection TL494 feedback received error amplifier inverting input, and connected to the inverting input of the reference, TI gives the official application is the same. Can it use the feedback received error amplifier inverting input, and then with reference to the input and PWM output transistors from the collector C to a pullup resistor connected to VCC output? Why do I use the BUCK circuit, there will be no output? Other feedback PWM control chip is connected to the inverting input terminal, and why 494 is an exception