I have to test a TPS65270 based buck regulator design with Vin=12V and Vout=3.3V/3A. The 3.3V output power rail has 4x220uF bulk capacitance. I'm using C39= 0.1uF (and not 0.01uF) cap on the SS2 pin (16msec ramp-up time) to compensate the inrush current and the switching frequency is around 600kHz. I'm looking for the right values of a Type III compensation circuit as part of the DVT. However, when tried to use the equations on page_14 of the datasheet, I get very different figures comparing to the values used in the original schematic and in the application examples I had a look. I have no idea at the moment why the equations don't work for me. Nevertheless, any advice to find the optimum values for R16, C32, C31 and C44 is much appreciated.