Hi
I am a student with little experience on such project. I want to use a charge pump to boost up the recertified voltage - typical 0.4V with 0.6-1.5mA current to 2.4V. So, is this possible to use bq25505 for this application? and Is there some example case or suggestion for that ?
By the way, it looks there is no internal voltage monitor to lock its output on certain voltage which is higher than 1.9V (VBAT_UV ). Is that means it must set VBAT_OK_HYST to make VBAT_OK control external PFET to turn on/ off load ?
If let VBAT_OK connect to EN2 of TPS62736, will TPS62736 turn off the input from bq25505 when VBAT_OK is low ?
Many thanks
Zheng