I am experiencing an issue with a PTB78560CAH blowing a Litttlefuse PICO II P/N: 0472001.MAT1L one amp fuse used as input protection to the DC/DC converter. The output load is under five milliamperes and consists of a 12 VDc brushless fan and electronic circuits. The PTB78560CAH is powered from an aircraft electrical system that uses generators and a lead acid gel battery as a power source with the source voltage between 26.5 VDC and 29.5 VDC; electrical loads in the aircraft that are operating when the PTB78560CAH is powered include several brush type electrical motors and a 400 Hz static inverter. The input has two 0.1 uF capacitors in parrallel and two Nichicon 100 uf 63 VDC PW series capacitors in parallel to the input.
Would increasing the fuse4 value to three amperes solve the problem, or is there another issue(s) that I should be thinking about.