how to improve Power factor, for led driver, am using tps92210,am getting 0.87 as PF ,can any one suggest me
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
how to improve Power factor, for led driver, am using tps92210,am getting 0.87 as PF ,can any one suggest me
sir,
but my knowledge is nill on pmp6023 which u mentioned here am using just tps92210 in constant on time mode control only, and u have pointed out phase shift delay because of reducing in output power with out emi cap values yes we have solved that problem and we have achieved 0.95 power factor,but sir can u tell me how exactly we need to design emi filters based on output power,
note and please tell why u are notifying abt pmp06023 where can i use that in IC in my circuit please tell me purpose of that IC
In generality if you leave the switching frequency the same, reduce the transformer inductance to get similar duty cycles at twice the power the peak currents will be twice as high or 6dB higher. If the wave shape remains the same the harmonics will be the same ratio regardless of power level. This means there will be 6dB higher harmonics reflected back to the input which would require 6dB more filtering. This is a generality, many other things change in a design that doubles the output power.
sir, once please clarify me design of filter across AC side and after diode brdige rectifier, am unable catch out the design
The PFC capacitor is on the rectified AC side of the rectifier bridge, the EMI X-capacitor can be before or after the rectifier bridge, if it is after it does not need to be X2 rated (X2 rated is typical for universal input 85-265). The capacitors on the input side of the rectifier bridge can be discharged by the connections to the line and neutral (either line or neutral can have negative current to discharge the capacitor). If it is on the rectified AC side the diodes block the line or neutral from discharging the capacitors. If the power circuit draws less than is needed to discharge the line and PFC capacitor it will hold up (not get to zero) causing a discontinuity. This will add to harmonic distortion. A power factor corrected circuit tends to draw much less current when the AC line is low meaning there isn't much current draw from the circuit to discharge the capacitors on the rectified AC side including the PFC capacitor.
sir you have told mehow harmoics occurs, but i need to know from hoe to design the fiter to reduce harmonics.