I'm using the bq51013B chip with a WR303050-15F5-G charging coil from TDK and followed the bq51013EVM schematic precisely. I am also using PN: bq500212A on the TX inductive side. Charging occurs without issue but the problem that I am having is that the Charge Complete signal does not seem to get transmitted to the TX coil once charging is done. I can clearly see the current to the battery drop to 0 yet the TX chip continues to stay in Power Transfer mode. How does the bq51013 chip determine Charge Complete and are there specific settings or COMMx capacitor values (currently using 22nF for each) that need to be set to enable communication between the chips?
Best,
Tom