Hi All,
I used webench to make a LM5175 design for Vin:6-42V Vout 12V@3A. But I got a problem. I simulated with different Vin voltages and I saw a problem…
- Vin:8V Vout:12V@3A Load ::: Output voltage is ok for this Vin.
- Vin:10V Vout:4-6V@3A Load ::: Output voltage is NOT ok for this Vin. It should be 12V, but simulation result is 4-6V…
- Vin:12V Vout:12V@3A Load ::: Output voltage is ok for this Vin. (Bigger Vin voltages are also ok.)
Maybe you can also reproduce the design and test these cases… Is this just a simulation error or design has a vin voltage gap? What can you advise me?
Note: 12V@6A webench design simulation has similar problem. Maybe there is another person who got this problem...
Thanks in advance....