Hey Team,
The specification says that we can sink 5A, and that was tested for a 200nS period. We have a matrix circuit that is being driven by a MOSFET that’s driven by the LM5111. The MOSFET is driving a 4V capacitive bus, and that bus remains charged-up when the MOSFET is turned-OFF. We are adding a switch that senses that the MOSFET is OFF, and then routing the charged bus through the switch to the same driver as drives the MOSFET through a 1 Ohm limiting resistor. This configuration discharges the charged bus with an approximately 1.5 uS time constant, >> 200 nS.
The question is how much more current can we pump into the output sink transistor of the LM5111 in order to discharge the charged bus more quickly. Keep in mind the discharge is an exponential decay, and we want to be as aggressive as possible slashing the value of the 1 Ohm series resistor.
Thanks!
Dylan Ashley