Hello
I had some basic question related to TPS65721 and I hope you could answer them. Please ignore if few question have been already answered in previous threads.
1. Can the MODE pin be left floating and the PWM or PFM mode be forced from I2C? Also Can the I2C write to MODE override if the MODE pin is connected to ground?
2. Is it alright to leave PB_IN_N pin pulled high. So that the device is shipped in powerdown mode and can be started once the charger is plugged in?
3. Is it beneficial to use a voltage divider from SYS to THRESHOLD pin to reset the device or can there be any problem if I grounded the threshold Pin?
Thanks