Hi,
My customer has question about TPS54320.
Could you tell us about question?
[Question]
My customer want to controll the EN pin by the external signal.
It is the High/Low signal that mean High(enable)=3.3V and Low(disable)=0V.
Datasheet say if an application requires controlling the EN pin, use an open-drain output logic to interface with the EN pin.
Can we input High/Low signal directly to the EN pin?
Is it required external parts?
Best Regards,
tateo