Hi,
In HPA-603 there are some questionswith the protector.
- Although R32=R34, R35=750k < R33. These resistors connects to net driving U4:A sleep mode comparator. Yet there is 1M R29 connecting with 3.3V VREF complicating voltage comparison. What is expected U4:A pin 3 voltage of the design?
- BAT connects to through R10, R28, R31 to VREF, but as in first question the net is also connects to U4:A pin 3 via R29.
These are not simple voltage divider. How should we calculate them?
Also on the lower right sheet format fields (with TI brand, title, Date) in the schematic the EVM is labeled as HV 48V; J2 header labeled as VOUT 0-50.4V; J1 header Vin is labeled 36-57V. Yet in 1.1 Introduction the evm is said for 8-cell battery.
We are unclear on the exact battery count suitable for the EVM. Also as we change input and battery count within the range the resistor values above needs to be updated. Please give us guide lines on how to calculate the values (we are aware of the spreadsheet for calculating components for bq2461x, just this network is a bit complex and wish to get guidance).
Matt