Hi,
Does anyone know LM5060 has over current protection when Output is shorted to ground? It is also called short circuit protection when load is shorted. In order to protect MOSFET, the driver should monitor Vds of MOSFET and Gate, when Vds of MOSFET and Gate are high in the same time, that is the short circuit condition, the driver then turns off MOSFET, that is most of other high side drivers do. I realized that LM5060 detects Vds of MOSFET, but I am not sure if there is short circuit protection to turn off MOSFET when load (OUTPUT pin) is shorted to ground.
Thanks!
John