Hello,
I designed with webench on tps54340 a couple of months ago and when i got to test the pcb according this design, the output voltage is less than it should be
- Output should be 5v with/without load and in the test - got 4.85v load 1A and 4.73v @load 2.09A):
In addition, i made a new webench simulaltion today with the same parameters and it gives a different valeus for Rcomp (24.9K instead of 26.1k) and Ccomp2 (20pf instead of 16pf) (all rest are the same).
Question - can Webench be trusted for correct designs outputs for selecting the correct valeus of ressistors and capacitors ets'?
byd, all tests made in lab with 25 celsiouse and proper conditions.
thank you in advance,