Hi all,
Would you mind if we ask TPS2041C, TPS2051C?
<Q1>
The datasheet shows "Additionally, bypassing the output with a 0.01-μF to 0.1-μF ceramic capacitor improves the immunity of the device to short-circuit transients."
What does "improves the immunity of the device to short-circuit transients" mean?
Does it mean a measure of transients using capacitance?
<Q2>
When our customer use this device as USB standard applications, is it required to definitely use 150uF for output capacitance?
Our customer wonder whether it is possible to use 10uF or 47uF capacitance for output capacitance or not.
So in this case, the condition of the Cout is 150µF about several test result on the datasheet.
If it used 10uF or 47uF, will the undershoot be bigger?
And the following is not out of range, is it?
"The voltage undershoot should be controlled to less than 1.5 V for 10 µs."
Kind regards,
Hirotaka Matsumoto