Similar questions have been asked by others but where not resolved.
I currently have the following evaluation hardware and software from a previous project.
EV2300/bq27510EVM HPA320 REV A
bqEVSW Ver 0.9.92
Now I want to evaluate and later create the golden DFI file for a new project that uses the bq27510-G3 fuel gauge, but the evaluation hardware and software are for the older chip.
What is the best way to proceed?
I have the bq27510-G3 Firmware Image file SENC V4.00. Should I update the firmware of the chip on the bq27510EVM?
Will this break bqEVSW Ver 0.9.92?
I have looked for updates to bqEVSW but have not found any.
I have heard of bqstudio. Will this software do what I want?
I think I could use bqEVSV and the above .senc file to install the bq27510-G3 firmware on the EVM. Then proceed to use bqstudio to create the golden DFI file. Is this the best way to go?