This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25010 not charging my battery

Other Parts Discussed in Thread: BQ25010

Hello Sir,

I'm facing some weird problem regarding charging of BQ25010.  When i connect USB cable it goes into charging mode for 1-2 seconds and then suddenly stops charging. I have checked  my connection CE pin is pulled low through 1M resistor and ISET2 pin is pulled high for 500ma charging current. Also my ISET1  pin is connected to 1.62k for precharging current of 50ma. Same circuit is working fine on another board but only facing this issue with some boards. 

STAT1 & STAT2 line voltage levels(pulled high using 1M resistor) 

STAT1 = 3.16V         STAT2 = 3.16V          (not charging & USB cable is disconnected)

STAT1 = 0V              STAT2 = 3.16V          (USB cable connected and remains only for 1-2 seconds)

STAT1 = 3.16V        STAT2 = 3.16V           (USB cable still connected)

Hope you guys can help me out with this situation.

Thanks,

Vishal