Hi,
We have this application where we are planning to use TPS7A7001 linear voltage regulator. In this application the OUTPUT voltage could be at 2.5V for ~30 seconds even after the input voltage has been removed. The maximum current the 2.5V net can provide is about 230mA.
Is it required to a diode between the INPUT and the OUTPUT pins of TPS7A7001 to protect the device from this reverse current or is it okay to leave it as is? The EN pin is controlled externally from a power detection circuit.