I have a 2S2P LION configuration and wanted to see how it recovers from Cell undervoltage. Discharged the pack below 5V and CUV and then CUCV were set as expected. Cell 1 recovered to 3208 mV and Cell 2 2543 mV. Charging status PV bit is still set but there is 0 current flowing. One curios thing VAC at the test connector is 1200mV but AC adapter voltage in the registers only shows 9100 mV. Eval is set up to use hardware precharge.