I cannot find any info about overcurrent protection in the above devises. There is only statement "Maximum continuous switch current is…". What will happen if this current will be exceeded?
TPS22963C has reverse current protection only while disabled. There is a remark in datasheet, it is to "… allow for intentional reverse current (when the switch is enabled) for some applications". Is it completely bidirectional having the same electrical parameters?
Can you recommend some simple load switch with overcurrent protection and adjustable current limit 0.2A to 1.5A?