Hi All,
We are currently working on a design integrating the TPS65910 with an AM3354 processor. This will be coupled with DDR3 RAM.
The TPS65910 must be configured to use BOOT1 = 0 / BOOT0 = 1. Otherwise the initial start-up voltage of VDD2_REG will cause fire :)
What this means is that the CK32K_CTRL Bit in the DEV_CTRL register will be configured to use an external crystal (or 32k square wave).
Section 6.4 of the users manual
"Switching from the 32-kHz crystal oscillator or external square-wave clock to the RC oscillator is not supported."
Questions:
1. If an external crystal is not available will the TPS65910 revert to using its internal oscillator?
2. If it does revert to the internal oscillator does it change the state of the CK32K_CTRL bit?
3. I'm assuming that the quoted paragraph above refers to switching while maintaining product operation? Can the register be changed and the product power cycled to change source? What is the behaviour when the register is changed? Does the TPS6910 crash?
Cheers, Sam